{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Do the FA100F or FA100S circuit breaker enclosures provide the capability to padlock the circuit breaker in either the ON or the OFF position?
Issue:
Product design features

Product line:
Circuit breaker enclosure

Resolution:
FA100F and FA100S enclosures provide an integral lock plate on the cover that allows the circuit breaker to be padlocked in the ON or OFF position. A handle padlock attachment, HPAFK, could also be purchased separately and field installed on the breaker to provide padlock capability in the ON or OFF positions.

Schneider Electric USA

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: