Question:
Which standards do the Multi 9 (M9) breakers meet?
Product Line:
Multi-9 Circuit Breakers
Resolution:
Following are the standards met:
UL 489 Circuit breaker file #E215117
UL 1077 Circuit Breaker File #E90509
CSA C22.2 No. 235-M89 file #LR80849
IEC 60947-2
VDE 0660
CE Marked
NOTE: These are the standards that the Multi-9 line uses. Not all of the breakers meet all of the above standards.
Which standards do the Multi 9 (M9) breakers meet?
Product Line:
Multi-9 Circuit Breakers
Resolution:
Following are the standards met:
UL 489 Circuit breaker file #E215117
UL 1077 Circuit Breaker File #E90509
CSA C22.2 No. 235-M89 file #LR80849
IEC 60947-2
VDE 0660
CE Marked
NOTE: These are the standards that the Multi-9 line uses. Not all of the breakers meet all of the above standards.