{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for a QMB365W, series E1 (may also be shown as E01)?
Issue:
What are the repair parts for a QMB365W, Series E1 (may also be shown as E01)?

Product Line:
Fusible QMB Switches

Resolution:
The repair parts for the QMB365W, series E1 (E01) are as follows. No other parts (enclosure, labels) are available.
Arc Suppressor Assembly - 4052031850 (3 required)
Arc Shield - 4052085601 (3 required)
Load Base Assembly - 4052112050 (3 required; includes lugs)
Load Base Mounting Screw - 2142720241 (3 required per load base)
Load Base Side Insulator - 4052098601 (1 required per load base)
Fuse Clamp Assembly per phase - line side - 4052031351 (two bolts included)
Fuse Clamp Assembly per phase - load side - 4052031350 (two bolts included)
Handle Knob Kit - 4028343550
Lug Assembly (per lug) - 4025128750
Lug Mounting Nut (per lug) - 2342702400

Schneider Electric USA

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: