{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are the FAL/FHL breakers DIN rail mountable?

Issue:
Are the FAL/FHL breakers DIN rail mountable?

Product Line:
FAL/FHL Molded Case Circuit Breakers

Resolution:
No, FAL/FHL breakers do not have a DIN rail mounting adapter available.

Powerpact B-frame breakers are able to be DIN rail mounted as standard.
Powerpact H & J frame 3 pole breakers can be DIN rail mounted with the use of DIN rail mounting kit S29305. It requires 15 mm depth on a 35 mm DIN rail and fits 3 pole module breakers only (not available in 2 pole).

DIN Rail

Schneider Electric USA

Attachment(s)
48940-239-01.pdf [112.81 KB]