undefined undefined
{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are accessories available for the 1 pole FDA, FGA, and FJA breakers?
Issue:
Are electrical accessories available for 1p (1 pole) FDA, FGA, and FJA circuit breakers?

Product Line:
Powerpact F-Frame Circuit Breakers

Resolution:
Yes, the one pole FDA, FGA, and FJA breakers are available with electrical accessories. However, it will expand their mounting height from 1.5" to 3".

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: