{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for the PAK10CTG, series E01 ServicePak power outlet panel?
Issue:
Repair parts list for PAK10CTG, series E01

Product Line:
Power Outlet Panels

Resolution:
Only the parts listed below are considered field replaceable.
Cover - 4054005101
Cover Mounting Screws - 2142717161 (2 required)
Interior Trim - 4054021101
Interior Trim Mounting Screw - 4020513001K (2 required)
Interior Assembly - 4054018450 (includes the base assembly, circuit breaker(s), and receptacle(s))
Base Assembly - 4054010650
Circuit Breaker - QO120GFI
Receptacle - 4054001450
Receptacle Mounting Screw - 2190312160 (1 required)
Ground Bar - 4023017155
Ground Bar Mounting Screw - 4020547201
Closing Cap - BCAP
Closing Cap Mounting Screw - 2142720241 (2 required)
Note: Covers and Interior Trims do not have labels applied.

Schneider Electric USA