{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the consumption of the control coil for 8502SG contactor?
Issue:
Consumption of the control coil for 8502SG contactor

Product Line:
NEMA Contactors and Overload Relays

Environment:
Type S Contactors

Resolution:
Series A - 2970 VA inrush and 212 VA sealed for 60 hertz or 2970 VA inrush and 250 VA sealed for 50 hertz. Series B - 1300 VA inrush and 14 VA sealed 50/60 hz. This also applies to all 8536SF, 8538SF, 8539SF, 8606SF, 8630SF, 8640SF, 8702SF, 8736SF, 8738SF, 8739SF, 8810SF, 8903SF, 8910SYD368, and 8940 Size 5 except ``NP`` devices.

Schneider Electric USA