Search FAQs
Is a UL 489 listed non-automatic switch available in the Masterpact NW frame?
Issue:
Needs UL 489 listed masterpact non-automatic switch
Product Line:
Air Circuit Breaker
Resolution:
No. An automatic switch (has a trip point to protect itself) is available with UL 489 and IEC 947-3 listings.
No. An automatic switch (has a trip point to protect itself) is available with UL 489 and IEC 947-3 listings.
A non-automatic switch (has no trip capability) is available with ANSI C37 certification, UL 1066 listing, and with IEC 947-3 listing.
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: