Issue:
How can I change the rating plug of a 3 pole PA/PH circuit breaker?
Product Line:
PA, PH, and PC breaker
Resolution:
The following part numbers were used to set the breaker to different amperages. They are now obsolete.
600 A - PA3600RC
700 A - PA3700RC
800 A - PA3800RC
1000 A - PA31000RC
1200 A - PA31200RC
1400 A - PA31400RC
1600 A - PA31600RC
1800 A - PA31800RC
2000 A - PA32000RC
How can I change the rating plug of a 3 pole PA/PH circuit breaker?
Product Line:
PA, PH, and PC breaker
Resolution:
The following part numbers were used to set the breaker to different amperages. They are now obsolete.
600 A - PA3600RC
700 A - PA3700RC
800 A - PA3800RC
1000 A - PA31000RC
1200 A - PA31200RC
1400 A - PA31400RC
1600 A - PA31600RC
1800 A - PA31800RC
2000 A - PA32000RC
Released for:Schneider Electric USA