{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the mounting screws for FA/FH breakers?
Issue:
What is the part number for the mounting screw kit for the FAL or FHL breaker?

Product Line:
Legacy FAL/FHL Unit Mount breakers

Resolution:
The part number of the mounting screw kit for 2 and 3 pole breakers is 4812422451. The kit has 4 pan head, self locking, 8-32 x 3" long screws.

NOTE: For 1 pole FAL and FHL breakers, the mounting screw kit is 4812432950, which is already obsolete with no available replacement.

Schneider Electric USA