Issue:
Need a delay on standard undervoltage relay (UVR) in breaker.
Product:
Circuit Breakers
Resolution:
Yes. Time delay modules can be used with the NW/NT UVR in the following voltages (NOTE: outputs are all DC voltages):
Adjustable:
Volts | Cat # |
48-60 Vac/dc | S33680 |
100-130 Vac/dc | S33681 |
200-240 Vac/dc | S33682 |
380-480 Vac/dc | S33683 |
Non-adjustable:
Volts | Cat # |
100-130 Vac/dc | S33684 |
200-240 Vac/dc | S33685 |
Released for:Schneider Electric USA