{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the handle ties for QO, QOB, and QOU breakers?
Issue:
What handle tie does Square D offer for QO, QOB and QOU breakers?

Product Line:
Breakers installed on QO load centers or NQ, NQO, NQOB, NQOD panelboards

Resolution:
•Catalog number QO1HT will tie 2 single-pole handles together. 

QO1HT
See instruction bulletin, 40271-902-05.

•For 3 single-pole breakers, use QO3HT.  This handle tie will fit on the QOU, but the padlock attachment will not fit on the QOU, Series 3 (low amp frame). The padlock attachment will work on the QOU, Series 1 in the 100 A frame however. 

QO3HT

See instruction bulletin, 48840-181-01.

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
move-arrow-top