Search FAQs
What are the standard single phase and three phase kVA ratings for Transformers by SquareD/Schneider Electric?
Issue:
Listing of standard Transformer kVA sizes
Product Line:
LV Transformers
Environment:
Applies to Low Voltage Transformers by SquareD/Schneider Electric
Cause:
Transformer kVA levels fall into standard sizing levels for single phase and three phase products
Resolution:
Single phase Low Voltage Transformers: 1, 1.5, 2, 3, 5, 7.5, 10, 15, 25, 37.5, 50, 75, 100, 167, 200, 250, 333 kVA There are some smaller standard sizes available only on stocked product as shown in section 14 of the Digest 178.
Three phase Low Voltage Transformers: 3, 6, 9, 15, 30, 45, 75, 112.5, 150, 225, 300, 500, 750 kVA.
Three phase Medium Voltage Transformers: 1000, 1500, 2000, 2500, 3000, 3750, 5000 kVA