{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What type of fuse is to be used in the 9070 Type T with field installed fuse block or Type TF control transformer?
Issue:
9070T and 9070TF Control Transformer Fuse type

Product Line:
LV Transformers

Environment:
9070T and 9070TF Control Transformer

Resolution:
1-1/2`` x 13/32`` fuses
Primary: Class CC time delay (rejection type)
Secondary: may be either rejection or non-rejection type
All fusing must be sized according to NEC Article 450-3

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.