{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.

How can we help you today?

Video: Can the BLANK meter socket/tenant breaker positions in an MP Meter-Pak or EZM branch device be modified in the field with a meter socket and tenant circuit breaker?

Article available in these languages: Spanish

Issue:
Product design

Product Line:
MP Meter Pak metering

Resolution:
No. The MP Meter-Pak units that are supplied with a BLANK position CANNOT be converted in the field to include an additional meter socket/tenant breaker in the blank position.
Also, any of the EZM branch devices that come with a BLANK position CANNOT be converted in the field to include an additional meter socket/tenant breaker in the blank position.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: