{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for a HU364RB, series E1 heavy duty safety switch?
Issue:
HU364RB Series E1 Field Replaceable Parts.

Product Line:
Safety Switches

Environment:
Heavy Duty Safety Switches

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 4056028350 (OBSOLETE WITHOUT REPLACEMENT)
Arc suppressor assembly - 4051270650 (3 required)
Lug assembly - 4025116251 (6 required)
Line base phase insulator - 4052025301 (2 required)
Cross bar insulator - 4051136101
Dust shield - 4051136201
Mechanism insulator - 4051137101
Line and load base mounting screws - 4020506501 (2 required per base)
Handle knob kit - 4028344050K

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more