Issue:
Repair parts list for H324AWK, series E1
Product Line:
Safety Switches
Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 4051256850 (arc suppressor is included)
Load base assembly - 40560-27650
Arc suppressor assembly - 4051270102
Lug assembly - 4056027050
Line base phase insulator - 4051137201
Cross bar insulator - 4051136101
Dust shield - 4051136201
Mechanism insulator - 4051137101
Line and load base mounting screws - 4020506501
Handle knob kit - 4028344050K