Issue:
The list of repair parts is needed for Safety Switch catalog number H364AWK, series F5.
Product Line:
Heavy Duty Safety Switch
Resolution:
The replacement parts for the H364AWK, series F5 (F05) are as follows. No other parts are available.
-Complete Line Base - 4056703550 (1 required; includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
-Line Base mounting screws - 4020546401 (6 required per line base)
-Load Base Assembly - 4056678250 (1 required per phase; includes phynolic base, lugs, and fuse clips)
-Load Base mounting screws - 4020546401 (2 required per load base)
-Arc Suppressor Assembly - 4056677550 (1 required per phase)
-Arc Suppressor mounting screw - 4020514501
-Lug Assembly - CL20F (includes 6 lugs; requires mounting screws)
-Lug Assembly mounting screw - 2140122240 (per lug)
-Switch Mechanism - 4056678650 (also requires interlock shaft gasket 4056786001)
-Switch Mechanism mounting screws- 2299940562 (2 required)
-Handle Assembly - 4056663550 (requires handle gasket 4056603101)
-Lockplate - 4056672101
-Lockplate mounting screws - 2299940562 (2 required)
The list of repair parts is needed for Safety Switch catalog number H364AWK, series F5.
Product Line:
Heavy Duty Safety Switch
Resolution:
The replacement parts for the H364AWK, series F5 (F05) are as follows. No other parts are available.
-Complete Line Base - 4056703550 (1 required; includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
-Line Base mounting screws - 4020546401 (6 required per line base)
-Load Base Assembly - 4056678250 (1 required per phase; includes phynolic base, lugs, and fuse clips)
-Load Base mounting screws - 4020546401 (2 required per load base)
-Arc Suppressor Assembly - 4056677550 (1 required per phase)
-Arc Suppressor mounting screw - 4020514501
-Lug Assembly - CL20F (includes 6 lugs; requires mounting screws)
-Lug Assembly mounting screw - 2140122240 (per lug)
-Switch Mechanism - 4056678650 (also requires interlock shaft gasket 4056786001)
-Switch Mechanism mounting screws- 2299940562 (2 required)
-Handle Assembly - 4056663550 (requires handle gasket 4056603101)
-Lockplate - 4056672101
-Lockplate mounting screws - 2299940562 (2 required)