Issue:
Replacement parts
Product Line:
Heavy Duty Safety Switch
Resolution:
The replacement parts for the H362, series F5 (F05) are as follows. No other parts are available.
Interior Kit - HSIF3606F (Includes line and load base assemblies, mechanism, arc suppressor, all mounting hardware, and instructions)
Line Base Assembly - 4056603850
Line Base Assembly Mounting Screws - (3) 4020515101
Load Base Kit - HLB3606F (Includes load base, mounting hardware and instructions)
Load Base Assembly - 4056604050 (Does NOT include mounting hardware or instructions, it is ONLY the load base).
Load Base Assembly Mounting Screws - (2) 4020515101
Arc Suppressor kit - HAS0610F (includes arc suppressor and mounting hardware)
Lug kit - AL0306F (includes 6 lugs)
Handle/Mechanism kit - HM0610F (includes handle, mechanism, lockplate, and mounting hardware)
Cover Latch – 4056607201
Cover Latch Spring - 4022304301
Replacement parts
Product Line:
Heavy Duty Safety Switch
Resolution:
The replacement parts for the H362, series F5 (F05) are as follows. No other parts are available.
Interior Kit - HSIF3606F (Includes line and load base assemblies, mechanism, arc suppressor, all mounting hardware, and instructions)
Line Base Assembly - 4056603850
Line Base Assembly Mounting Screws - (3) 4020515101
Load Base Kit - HLB3606F (Includes load base, mounting hardware and instructions)
Load Base Assembly - 4056604050 (Does NOT include mounting hardware or instructions, it is ONLY the load base).
Load Base Assembly Mounting Screws - (2) 4020515101
Arc Suppressor kit - HAS0610F (includes arc suppressor and mounting hardware)
Lug kit - AL0306F (includes 6 lugs)
Handle/Mechanism kit - HM0610F (includes handle, mechanism, lockplate, and mounting hardware)
Cover Latch – 4056607201
Cover Latch Spring - 4022304301