Issue:
Repair parts
Product Line:
Double Throw Safety Switch
Resolution:
The repair parts for the DTU322, series F5 (F05) are as follows. No other parts are available.
-Line Base - 4056624250 (one each upper and lower; arc suppressor, load lugs, and wire assembly not included)
-Line Base mounting screws - 4020515101 (3 required per line base)
-Arc Suppressor Assembly - 4056635550 (1 required per line base)
-Arc Suppressor mounting screw - 4020514501 (1 required per arc suppressor)
-Wire Assembly- 4056732650 (1 required per phase; includes cable factory connected mechanical lug at one end and at other end a crimped connector; use lug mounting screws)
-Line and Load Lug Assembly - 4025101652 (per lug - line, load)
-Line, Load Lug mounting screw - 4020514202
-Ground Lug - 4025101652 (per lug)
-Ground Lug mounting screw - 4020513503
-Switch Mechanism - 4056646950 (each for upper and lower)
-Linkage Assembly - 4056682750
-Linkage Assembly mounting screws - 2299940562 (7 required)
-Handle - 4056688750
-Lockplate - 4056673301
-Lockplate mounting screws - 2299940562 (2 required)
-Cover Latch - 4056607201 (each for upper and lower; also requires cover latch spring)
-Cover Latch Spring - 4022304301 (each for upper and lower; also requires cover latch)
Repair parts
Product Line:
Double Throw Safety Switch
Resolution:
The repair parts for the DTU322, series F5 (F05) are as follows. No other parts are available.
-Line Base - 4056624250 (one each upper and lower; arc suppressor, load lugs, and wire assembly not included)
-Line Base mounting screws - 4020515101 (3 required per line base)
-Arc Suppressor Assembly - 4056635550 (1 required per line base)
-Arc Suppressor mounting screw - 4020514501 (1 required per arc suppressor)
-Wire Assembly- 4056732650 (1 required per phase; includes cable factory connected mechanical lug at one end and at other end a crimped connector; use lug mounting screws)
-Line and Load Lug Assembly - 4025101652 (per lug - line, load)
-Line, Load Lug mounting screw - 4020514202
-Ground Lug - 4025101652 (per lug)
-Ground Lug mounting screw - 4020513503
-Switch Mechanism - 4056646950 (each for upper and lower)
-Linkage Assembly - 4056682750
-Linkage Assembly mounting screws - 2299940562 (7 required)
-Handle - 4056688750
-Lockplate - 4056673301
-Lockplate mounting screws - 2299940562 (2 required)
-Cover Latch - 4056607201 (each for upper and lower; also requires cover latch spring)
-Cover Latch Spring - 4022304301 (each for upper and lower; also requires cover latch)
Released for:Schneider Electric USA