Issue:
Repair parts
Product Line:
Double Throw Safety Switch
Resolution:
The repair parts for the DT362, series F5 (F05) are as follows. No other parts are available.
-Line Base - 4056603850 (1 each upper and lower; arc suppressor and wire assembly not included)
-Line Base mounting screws - 4020515101 (3 required per line base)
-Load Base - 4056683450 (1 each upper and lower; wire assembly not included)
-Load Base mounting screws - 4020515101 (2 required per load base)
-Arc Suppressor Assembly - 4056635550 (1 required per line base)
-Arc Suppressor mounting screw - 4020514501 (1 required per arc suppressor)
-Wire Assembly - 4056609750 (1 required per phase; includes cable factory connected mechanical lug at one end and a crimped connector at other end)
-Line and Load Lug Assembly - 4025101652 (per lug)
-Line, Load Lug mounting screw - 4020514202
-Ground Lug - 4025101652 (per lug)
-Ground Lug mounting screw - 4020513503
-Switch Mechanism - 4056646950 (1 each for upper and lower)
-Linkage Assembly - 4056614950
-Linkage Assembly mounting screws - 2299940562 (7 required)
-Handle - 4056688750
-Lockplate - 4056673301
-Lockplate mounting screws - 2299940562 (2 required)
-Cover Latch - 4056607201 (1 each for upper and lower; also requires cover latch spring)
-Cover Latch Spring - 4022304301 (1 each for upper and lower; also requires cover latch)
Repair parts
Product Line:
Double Throw Safety Switch
Resolution:
The repair parts for the DT362, series F5 (F05) are as follows. No other parts are available.
-Line Base - 4056603850 (1 each upper and lower; arc suppressor and wire assembly not included)
-Line Base mounting screws - 4020515101 (3 required per line base)
-Load Base - 4056683450 (1 each upper and lower; wire assembly not included)
-Load Base mounting screws - 4020515101 (2 required per load base)
-Arc Suppressor Assembly - 4056635550 (1 required per line base)
-Arc Suppressor mounting screw - 4020514501 (1 required per arc suppressor)
-Wire Assembly - 4056609750 (1 required per phase; includes cable factory connected mechanical lug at one end and a crimped connector at other end)
-Line and Load Lug Assembly - 4025101652 (per lug)
-Line, Load Lug mounting screw - 4020514202
-Ground Lug - 4025101652 (per lug)
-Ground Lug mounting screw - 4020513503
-Switch Mechanism - 4056646950 (1 each for upper and lower)
-Linkage Assembly - 4056614950
-Linkage Assembly mounting screws - 2299940562 (7 required)
-Handle - 4056688750
-Lockplate - 4056673301
-Lockplate mounting screws - 2299940562 (2 required)
-Cover Latch - 4056607201 (1 each for upper and lower; also requires cover latch spring)
-Cover Latch Spring - 4022304301 (1 each for upper and lower; also requires cover latch)
Released for:Schneider Electric USA