{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
On an NF 250A main breaker panelboard, can the main breaker be changed to one with a different rating such as 150A using a KAL36150 instead of a KAP36150?
Issue:
can the main breaker be changed to one with a different rating such as 150A using a KAL36150 instead of a KAP36150?

Product Line:
Panelboards

Environment:
NF Panelboards

Resolution:
Yes. The lugs on one side of the new breaker will need to be removed so the mounting pads are exposed. The termination insert kit (AL250KAIN) from the existing breaker will need to be reinstalled on the new breaker. Keep in mind that when reattaching the breaker to the busbars using the hard bus connectors the handle of the main breaker must go in the up position when the breaker is energized.

Schneider Electric USA