Issue:
What is the coil replacement for class 8910 Type DPA12_?
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
8910 DPA Contactors
Resolution:
31074-400-38 for 60 hertz or 31074-400-39 for 50 hertz, coil consumption is 700 VA inrush, 46 VA sealed for 60 hertz applications or 678 VA inrush, 47 VA sealed for 50 hertz applications.
See attached for all other voltages.
What is the coil replacement for class 8910 Type DPA12_?
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
8910 DPA Contactors
Resolution:
31074-400-38 for 60 hertz or 31074-400-39 for 50 hertz, coil consumption is 700 VA inrush, 46 VA sealed for 60 hertz applications or 678 VA inrush, 47 VA sealed for 50 hertz applications.
See attached for all other voltages.
Released for:Schneider Electric USA