{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are replacement control coils available for 8965RO hoist contactors?
Issue:
Replacement coil kits for the 8965RO contactors.

Product Line:
8965 Hoist Contactors

Environment:
North American Products

Cause:
Maintenance

Resolution:
Select the replacement kit for the 8965RO10 -11 -12 and -13 from the table below based on voltage and frequency.
Note:
Coils with prefix 31002-403 are tape-wound coils with slip-on terminals,packaged in quantities of two, and include a wire jumper.
Coils with prefix 31002-400 are molded coils with saddle clamp screw terminals, packaged individually.

Example:  Replacement coil for 8965RO12V21.
Answer:  31002-400-47
Coil PrefixHzAC Coil Suffix
24V110-115V120V208-220V240V480V550V600V
31002-403-60193940-----
31002-400----4749585960
31002-403-50-40------
31002-400----4951-60-

Schneider Electric USA