{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What class of fuse do ALL the 800 A and 1200 A heavy duty safety switches accept?
Issue:
Product design features

Product line:
Heavy Duty Safety Switches

Resolution:
The 800 A and 1200 A heavy duty safety switches accept class L fuses ONLY. With class L fuses installed, the switches are UL listed for use on systems with up to 200,000 RMS symmetrical amperes available fault current.

NOTE: DO NOT USE RENEWABLE LINK FUSES IN SQUARE D SAFETY SWITCHES. The use of renewable link fuses may adversely affect user safety, impair reliability and will void the warranty.
NOTE: Class L fuse is a 600 V construction fuse that is used in the 240 V rated switches

Schneider Electric USA

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.