{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for an H368NR, Series E4 heavy duty safety switch?
Issue:
What are the replacement parts for an H368NR, Series E4?

Product Line:
HD Safety Switch

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 4401139255 (3 required; arc suppressor assembly not included)
Load base assembly - 4401139351 (3 required)
Arc suppressor assembly - 4401139450 (3 required)
Lug assembly - 4405005402 (1 required per base assembly)
Neutral assembly - H1200SNE4
Line base phase barrier - 4401119501 (2 required)
Line base insulating plug - 4401133901
Handle assembly - 4401141351
Door thumb retainer - 4405049001
Door thumb screw - 4405043401
Handle knob kit - 4028343550
Neutral bonding strap - 4401134250SEL
Crossbar Insulator Kit - 4051275250 (metal crossbar is not replaceable)
Fuse Mounting Hardware - Bolt = 2140128481, Nut = 2342702800, Washer = 2360100280

Schneider Electric USA