{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are hermetically sealed contact blocks?
Issue:
What does hermetically sealed indicate in reference to the 9001KA* contact blocks?

Product Line:
30 mm Push Buttons

Environment:
Type K, SK and KX Electrical Components

Resolution:
The contact is sealed in a glass tube. No hazardous gas or particles can get into the contact.

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: