{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for the H323N, series F3? (may be shown as F03)
Issue:
Repair parts

Product Line:
HD Safety Switch

Resolution:
The repair parts for the H323N, series F3 (F03) are as follows. No other parts are available.
Interior kit - HSIF310F (includes line and load base assemblies, mechanism, arc suppressor, all mounting hardware, and instructions)
Load base kit - HLB310F (includes load base and mounting hardware)
Arc Suppressor kit - HAS0610F (includes arc suppressor and mounting hardware)
Lug kit - AL10F (kit includes 6 lugs)
Handle/Mechanism kit- HM0610F (kit includes handle, mechanism, lockplate, and mounting hardware)
Neutral Assembly - SN0610 (includes neutral assembly and bonding screw)
Neutral bonding screw - 4028365650

Schneider Electric USA

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: