{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for the HU361AWK, series F1? (may be shown as F01)
Issue:
old design repair parts

Product Line:
Heavy Duty Safety Switches

Resolution:
The repair parts for the HU361AWK, series F1 (F01) are as follows. No other parts are available.
Line Base Assembly - 4056643050 (1 required; arc suppressor assembly not included)
Arc Suppressor Assembly - 4056669451 (1 required)
Lug Assembly - CL0306F (includes 6 lugs)
Switch Mechanism - 4056610750
Handle Assembly - 4056684150K
Handle Gasket - 4056603101
Lockplate - 4056637601
Line base mounting screw - 4020516001 (3 required)
Arc Suppressor mounting screw - 4020514501 (1 required)
Lockplate mounting screw - 2299940562 (2 required)

Schneider Electric USA

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: