Issue:
Product design features
Product Line:
Meter Pak Metering
Resolution:
The MP22125, MPR22125 and MPH22125 accepts the following wire size and range - (1) #4 - 250kcmil Al/Cu wire Per Phase and Neutral.
There are NO Alternate lugs for these Meter-Pak catalog numbers.
The MP33125, MP44125, MP55125, MP66125, MPR33125, MPH33125, MPR44125, MPH44125, MPR55125, MPH55125, MPR66125 and MPH66125 contains the standard lug kit MMLK250 and accepts the following standard wire size and range; (1) #1/0 - 600kcmil Al/Cu wire OR (2) #1/0 - 250kcmil Al/Cu wire.
The Alternate lugs for these Meter-Pak devices are:
1) Lug kit MMLK500 (accepts (2) #3/0 - 500kcmil Al/Cu Wires per phase)
2) Lug kit MMLK600 (accepts (2) #2 - 600kmcil Al/Cu Wires per phase)
3) For the below alternate lugs, MUST use the lug landing kit MMSK2.
NOTE: The Anderson lugs are Compression lugs and the ILSCO lugs are Mechanical lugs.
Product design features
Product Line:
Meter Pak Metering
Resolution:
The MP22125, MPR22125 and MPH22125 accepts the following wire size and range - (1) #4 - 250kcmil Al/Cu wire Per Phase and Neutral.
There are NO Alternate lugs for these Meter-Pak catalog numbers.
The MP33125, MP44125, MP55125, MP66125, MPR33125, MPH33125, MPR44125, MPH44125, MPR55125, MPH55125, MPR66125 and MPH66125 contains the standard lug kit MMLK250 and accepts the following standard wire size and range; (1) #1/0 - 600kcmil Al/Cu wire OR (2) #1/0 - 250kcmil Al/Cu wire.
The Alternate lugs for these Meter-Pak devices are:
1) Lug kit MMLK500 (accepts (2) #3/0 - 500kcmil Al/Cu Wires per phase)
2) Lug kit MMLK600 (accepts (2) #2 - 600kmcil Al/Cu Wires per phase)
3) For the below alternate lugs, MUST use the lug landing kit MMSK2.
NOTE: The Anderson lugs are Compression lugs and the ILSCO lugs are Mechanical lugs.
Released for:Schneider Electric USA
Issue:
Product design features
Product Line:
Meter Pak Metering
Resolution:
The MP22125, MPR22125 and MPH22125 accepts the following wire size and range - (1) #4 - 250kcmil Al/Cu wire Per Phase and Neutral.
There are NO Alternate lugs for these Meter-Pak catalog numbers.
The MP33125, MP44125, MP55125, MP66125, MPR33125, MPH33125, MPR44125, MPH44125, MPR55125, MPH55125, MPR66125 and MPH66125 contains the standard lug kit MMLK250 and accepts the following standard wire size and range; (1) #1/0 - 600kcmil Al/Cu wire OR (2) #1/0 - 250kcmil Al/Cu wire.
The Alternate lugs for these Meter-Pak devices are:
1) Lug kit MMLK500 (accepts (2) #3/0 - 500kcmil Al/Cu Wires per phase)
2) Lug kit MMLK600 (accepts (2) #2 - 600kmcil Al/Cu Wires per phase)
3) For the below alternate lugs, MUST use the lug landing kit MMSK2.
NOTE: The Anderson lugs are Compression lugs and the ILSCO lugs are Mechanical lugs.
Product design features
Product Line:
Meter Pak Metering
Resolution:
The MP22125, MPR22125 and MPH22125 accepts the following wire size and range - (1) #4 - 250kcmil Al/Cu wire Per Phase and Neutral.
There are NO Alternate lugs for these Meter-Pak catalog numbers.
The MP33125, MP44125, MP55125, MP66125, MPR33125, MPH33125, MPR44125, MPH44125, MPR55125, MPH55125, MPR66125 and MPH66125 contains the standard lug kit MMLK250 and accepts the following standard wire size and range; (1) #1/0 - 600kcmil Al/Cu wire OR (2) #1/0 - 250kcmil Al/Cu wire.
The Alternate lugs for these Meter-Pak devices are:
1) Lug kit MMLK500 (accepts (2) #3/0 - 500kcmil Al/Cu Wires per phase)
2) Lug kit MMLK600 (accepts (2) #2 - 600kmcil Al/Cu Wires per phase)
3) For the below alternate lugs, MUST use the lug landing kit MMSK2.
NOTE: The Anderson lugs are Compression lugs and the ILSCO lugs are Mechanical lugs.
Released for:Schneider Electric USA