{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
How many coils are included with the part number 31002-403?
Issue:
What is 31002-403-** coil part #?

Product Line:
NEMA and Definite Purpose Contactor and Starter

Environment:
8965 Reversing Hoist Contactor

Resolution:
This is a coil set.  Two coils are supplied along with a jumper wire to connect the coil "commons" together; for 31002-403-19 (24 volt 60 hertz) or 31002-403-40 (120 volt 60 hertz / 110 volt 50 hertz) for use with the 8965RO reversing hoist contactor.

Schneider Electric USA