{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is a solid neutral assembly?
Issue:
What is a solid neutral assembly?

Product Line:
Distribution Equipment

Resolution:
A solid neutral assembly is an unswitched component used with voltage systems that include a grounded conductor (neutral). It will consist of lugs for incoming and outgoing grounded conductors (neutrals) and a lug for the grounding conductor (if the device is used as service equipment). For service equipment use, the neutral assembly would be bonded to the enclosure with a bonding screw or strap supplied with the equipment.

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: