{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the part number for the protective boots for 9001 type K and SK operators?

Issue:
Protective boots for 9001K and 9001SK operators

Product Line:
30MM push buttons and operators

Environment:
Class 9001 Type K/SK Operators

Resolution:
The boots are part numbers 9001KU1 thru 9001KU8 depending on color required, see table below for selection:

Protective Boots

For Non-Illuminated
Push Buttons [9]

Clear Color for

Type [2]

Color

Type [2]

Black

KU1

Standard knob selector switch

KU17

Red

KU2

Gloved-hand cap for use on standard knob selector switch

KU18

Blue

KU3

Brown

KU4

Green

KU5

Standard pilot light and maintained contact push buttons

KU27

Yellow

KU6

Clear

KU7

Clear

KU8

Push-to-test and illuminated push button without guard

KU37

(Provides Full Guard)

Illuminated push button with guard

KU47

NOTE: These Type KU protective boots are recommended for very dirty environments or severe hose down, but they are not required for UL Type 4 rating on the Type K operators or UL Type 4 or 4X rating on the Type SK operators. The K1 wrench (see Wrenches for Type K and SK Operators) is required for installation of these boots.


Schneider Electric USA