Search FAQs
What plug is required for use with the receptacle used on HU362WA, HU362DSWA, HU362CSWA, and HU362AWA (safety switches with Appleton POWERTITE receptacles installed)?
Issue:
Selection
Product Line:
HD SS
Resolution:
The receptacle is UL Listed for use with Square D or Appleton plug ACP6034BC. It is also UL Classified for use with Square D or Crouse-Hinds ARKTITE plug APJ6485.
Selection
Product Line:
HD SS
Resolution:
The receptacle is UL Listed for use with Square D or Appleton plug ACP6034BC. It is also UL Classified for use with Square D or Crouse-Hinds ARKTITE plug APJ6485.
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: