Issue:
Product Design Features.
Product Line:
General Duty, Heavy Duty and Double Throw Safety Switches
Resolution:
There are NO internal barrier kits available for general duty or double throw switches. The internal barrier kits are ONLY available for heavy duty safety switches.
NOTE: The internal barrier kits are NOT the same thing as the line side service entrance barriers to meet the NEC requirements for service entrance applications.
The following internal barrier kits are available for heavy duty safety switches ONLY:

NOTE: For the use of Load Side Barrier to be used on the 400 A through 1200 A, it requires the line side barrier to be installed
Product Design Features.
Product Line:
General Duty, Heavy Duty and Double Throw Safety Switches
Resolution:
There are NO internal barrier kits available for general duty or double throw switches. The internal barrier kits are ONLY available for heavy duty safety switches.
NOTE: The internal barrier kits are NOT the same thing as the line side service entrance barriers to meet the NEC requirements for service entrance applications.
The following internal barrier kits are available for heavy duty safety switches ONLY:
NOTE: For the use of Load Side Barrier to be used on the 400 A through 1200 A, it requires the line side barrier to be installed
Released for:Schneider Electric USA
Issue:
Product Design Features.
Product Line:
General Duty, Heavy Duty and Double Throw Safety Switches
Resolution:
There are NO internal barrier kits available for general duty or double throw switches. The internal barrier kits are ONLY available for heavy duty safety switches.
NOTE: The internal barrier kits are NOT the same thing as the line side service entrance barriers to meet the NEC requirements for service entrance applications.
The following internal barrier kits are available for heavy duty safety switches ONLY:

NOTE: For the use of Load Side Barrier to be used on the 400 A through 1200 A, it requires the line side barrier to be installed
Product Design Features.
Product Line:
General Duty, Heavy Duty and Double Throw Safety Switches
Resolution:
There are NO internal barrier kits available for general duty or double throw switches. The internal barrier kits are ONLY available for heavy duty safety switches.
NOTE: The internal barrier kits are NOT the same thing as the line side service entrance barriers to meet the NEC requirements for service entrance applications.
The following internal barrier kits are available for heavy duty safety switches ONLY:
NOTE: For the use of Load Side Barrier to be used on the 400 A through 1200 A, it requires the line side barrier to be installed
Released for:Schneider Electric USA