Issue:
Proper grounding of a low-voltage Transformer
Proper grounding of a low-voltage Transformer
Product Line:
LV Transformers
Environment:
Applies to all SquareD/Schneider Electric Transformers
Applies to all SquareD/Schneider Electric Transformers
Cause:
Proper Grounding of Transformers and other Electrical Equipment is a common topic when Transformers are installed or maintained.
Proper Grounding of Transformers and other Electrical Equipment is a common topic when Transformers are installed or maintained.
Resolution:
Square D LVGP Product Marketing/Support and CIC does/can not comment on grounding, other than to point the customer in the direction of the requirements in the National Electrical Code (NEC.) Any questions should be pointed in that direction, or the local AHJ (Authority Having Jurisdiction, commonly known as the inspector.)
Released for:Schneider Electric USA