Issue:
Differentiating Plug-On/Non-Plug-On Neutral Homeline™ Breakers & Panels
Product line:
HOM branch circuit breakers
Resolution:
LC = Load Center
PoN = Plug-On Neutral
HOM = Homeline
The standard, HOM, HOM-CAFI(Non-PoN white neutral wire), HOM-DF(Non-PoN white neutral wire), HOM-GFI(Non-PoN white neutral wire), HOM-EPD(Non-PoN white neutral wire) and HOM-HM branch circuit breakers can be installed in ALL HOM load centers.
The HOMT tandem breakers can ONLY be installed in the HOM load centers that are designed to accept the HOMT Tandem breakers (See FA101280 to determine if a HOM, LC accepts tandems)
The HOM, PoN(NO White neutral Wire) Arc Fault, Ground Fault and Dual Function Breakers can ONLY be installed in the HOM, PoN designed Load Centers
Below is a graphic visual of the Standard HOM and HOMT branch breakers being installed on the interior of a Standard HOM load center.
This information is available in the below attached instruction bulletin.

Attached is a video showing the installation of the standard HOM and the Plug-On Neutral Arc fault and/or dual function breakers being installed in the HOM load centers.

NOTE: PLEASE MAKE SURE FOLLOW ALL THE SAFETY INFORMATION PROVIDED AND NEVER WORK ON ENERGIZED EQUIPMENT.
Differentiating Plug-On/Non-Plug-On Neutral Homeline™ Breakers & Panels
Product line:
HOM branch circuit breakers
Resolution:
LC = Load Center
PoN = Plug-On Neutral
HOM = Homeline
The standard, HOM, HOM-CAFI(Non-PoN white neutral wire), HOM-DF(Non-PoN white neutral wire), HOM-GFI(Non-PoN white neutral wire), HOM-EPD(Non-PoN white neutral wire) and HOM-HM branch circuit breakers can be installed in ALL HOM load centers.
The HOMT tandem breakers can ONLY be installed in the HOM load centers that are designed to accept the HOMT Tandem breakers (See FA101280 to determine if a HOM, LC accepts tandems)
The HOM, PoN(NO White neutral Wire) Arc Fault, Ground Fault and Dual Function Breakers can ONLY be installed in the HOM, PoN designed Load Centers
Below is a graphic visual of the Standard HOM and HOMT branch breakers being installed on the interior of a Standard HOM load center.
This information is available in the below attached instruction bulletin.
Attached is a video showing the installation of the standard HOM and the Plug-On Neutral Arc fault and/or dual function breakers being installed in the HOM load centers.
NOTE: PLEASE MAKE SURE FOLLOW ALL THE SAFETY INFORMATION PROVIDED AND NEVER WORK ON ENERGIZED EQUIPMENT.
Released for:Schneider Electric USA