Issue:
Installing a PQ4610G plug-in unit on a vertically mounted Busway.
Product Line:
I-Line NEMA Busway
Environment:
Busplug flexibility in mounting
Cause:
Due to the various Busway run layout configurations, a Vertical Riser is used. The horizontally mounted Busway Busplugs are normally mounted perpendicular to the Busway .
Resolution:
The 30A, 60A, and 100A fusible plug-in units CAN be used on Busway mounted horizontally or vertically.
Released for:Schneider Electric USA