{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are dual voltage coils available for the TeSys D-line contactors?
Issue:
Are dual voltage coils available for the Tesys D, LC1D and LC2D, contactors?

Product Line:
IEC contactors and starters

Environment:
Products sold and used in the United States

Cause:
Dual voltage coil required

Resolution:
The standard TeSys D offer does not include dual voltage coils, these devices can only be provided with dual frequency (50/60Hz) coils.

We do have the TeSys D Green Offer which has an expanded range of coils for AC and DC voltages as follows: 24-60V 48-130V 100-250V and a coil for 250-415VAC / 250-500VDC

For more information see our TeSys D catalog at the following link: ohttps://www.se.com/us/en/download/document/LVCATESDELEC-EN/




Schneider Electric USA