{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Is the 8903 LX lighting contactor available in NEMA 3R type enclosure?
Issue:
Are Lighting contactors 8903LX available in NEMA 3R Enclosures?

Product Line:
NEMA Lighting Contactors

Environment:
Products sold and used in the United States

Resolution:
The 8903 Type LX lighting contactors are not available from the factory or warehouse already installed in NEMA 3R enclosures. You can order the open style contactor and the 9991 SDH1 enclosure separately and install them in the field.

Schneider Electric USA