{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What surface mount NEMA 1 general-purpose enclosure should be used with a Class 8903LO or 8903LXO?
Issue:
Need the surface mount NEMA 1 general-purpose enclosure should be used with a Class 8903LO or 8903LXO

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
NEMA Lighting Contactor

Cause:
Separate enclosure needed

Resolution:
Class 9991 Type LXG1. This is also the replacement enclosure for the 8903 type LXG and LG.

Schneider Electric USA