{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What certifications do the QOU breakers meet?
Product line:
Circuit breakers

Resolution:
Square D brand QOU breakers comply with:
• UL Standard 489 (File E84967)
• NEMA Standard AB1
• Canadian Standards Association CSA C22.2 No. 5-02
• IEC 60947-2
• CE

Square D brand QOU non-automatic switches comply with:
• UL Standard 489 (File E84967)
• Canadian Standards Association CSA C22.2 No. 5-02

Schneider Electric USA