{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Do the QOM1 and QOM2 main breaker kits require any pole spaces when installed on a convertible, QO or Homeline main lug load center interior?
Issue:
Does the QOM main breakers require pole spaces when installed on a convertible main lug load center interior?

Product Line:
QO and Homeline load centers

Resolution:
No, the main circuit breaker kits do NOT require any pole spaces. They are NOT a branch mounted device and do not require branch circuit breaker mounting spaces.

Schneider Electric USA