{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
In a 9001B control station are the contacts momentary or maintained?
Issue:
Are the contacts maintained or momentary on a 9001B control stations?

Product Line:
9001B Control Stations

Environment:
NEMA Control Stations and Enclosures

Resolution:
They are momentary unless explicitely specified as maintained in the digest or a selector switch.
Contact symbols 1, 3, 8, 16, 25, 109, 145, and 146 are momentary.
Contact symbols 10, 17, and 19 are maintained.

Schneider Electric USA