{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
On 10 - 30 A QO/QOB breakers, is there a suffix that can be added to breaker to allow them to accept larger wires?
Issue:
Can 10 - 30 A QO/QOB breakers be modified in the factory to accept larger wires?

Product Line:
Miniature Circuit Breakers

Resolution:
Suffix 5219 gives the breaker the lugs for 35 - 70 A breakers, which accepts #8 to #2 AWG Al/Cu wires.

Note: This suffix can only be applied on QO/QOB breakers and are not available on QOB-VH breakers

Schneider Electric USA