{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can the X and XD Wiring Devices use aluminum wire?

X and XD Series wiring devices can only be used with copper wire. These wiring devices can be used with copper-clad aluminum wire in the US market, which is recognized by both the NEC and UL as Copper Wire. Please refer to the Do X Series Wiring Devices support copper-clad aluminum (CCA)? for more details.

Schneider Electric USA