{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Modicon M340 maximum INT values

Issue

Customer needs to count up past 32,768 using a single 16 bit word.

Product Line

Modicon M340, Control Expert, Unity Pro

Resolution

The INT has a maximum value of 32767 because it uses the signed bit to support a data range of -32768 to +32767.

The UINT has a maximum value of 65535 because it is unsigned and uses all bits for a supported range of 0-65535.

Select the INT data type for your variable and you will be able to support 0-65535 using a single 16 bit word.

Schneider Electric USA

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Explore more
Range: