Please refer to the table below for maintenance kits for valve 7313. Please note that the valve repair kit includes replacement packing and stem and plug assembly.
Valve body part number | Replacement packing assembly | Packing wrench | Valve repair kit |
VB-7313-0-4-02 | YBA-622-2 | TOOL-20-1 | RYB-731-02 |
VB-7313-0-4-04 | YBA-622-2 | TOOL-20-1 | RYB-731-04 |
VB-7313-0-4-06 | YBA-622-2 | TOOL-20-1 | RYB-731-06 |
VB-7313-0-4-08 | YBA-622-2 | TOOL-20-1 | RYB-731-08 |
VB-7313-0-4-09 | YBA-622-2 | TOOL-20-1 | RYB-731-09 |
VB-7313-0-4-10 | YBA-622-2 | TOOL-20-1 | RYB-731-10 |
VB-7313-0-4-11 | YBA-622-2 | TOOL-20-1 | RYB-731-11 |