{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the 400, 600, and 800 amp factory supplied main breaker in the HCI Main Circuit Breaker I-Line panel?

Issue:

Main breaker part numbers for the 400,600 and 800 amp HCJ I-Line panel

Product Line:

Square D panelboard.

Environment:

Product Features

Resolution:

The current vertically mounted main breaker in a HCJ I-Line panel for 400, 600 and 800A is as follows:

The 400A has the LAP36400MB

The 600A has the MGP36600

The 800A has the MGP36800

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: