{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Video: How to use temporized start-stop with ATVLogic on ATV320 ?
This video showcases ATV Logic through an example of temporized start-stop with ATV320.
ATV Logic is reachable using SoMove FDT with ATV320 DTM
You can download the latest version of SoMove FDT and ATV320 DTM


🔔 VIDEO Timestamps :
0:06 - Introduction
1:21 - Program with ATV Logic
5:30 - Program explanation
6:48 - Add personalized settings in My Menu
7:49 - Check the program and transfer it to the drive
9:25 - Run the program
9:55 - Operational mode

➡️ For more information see:
• ATV320 - ATV Logic manual NVE71954 (English), NVE71955 (French), NVE71957 (German), NVE71959 (Spanish), NVE71958 (Italian), NVE71960 (Chinese)
Or press "F1" when you are inside the ATV Logic zone in the ATV320 DTM

• ATV320 Programming manual NVE41295 (English), NVE41296 (French), NVE41297 ​​​​​​​(German), NVE41298 (Spanish), NVE41299 ​​​​​​​(Italian), NVE41300 (Chinese)

Schneider Electric USA

Video: How to use temporized start-stop with ATVLogic on ATV320 ?
This video showcases ATV Logic through an example of temporized start-stop with ATV320.
ATV Logic is reachable using SoMove FDT with ATV320 DTM
You can download the latest version of SoMove FDT and ATV320 DTM


🔔 VIDEO Timestamps :
0:06 - Introduction
1:21 - Program with ATV Logic
5:30 - Program explanation
6:48 - Add personalized settings in My Menu
7:49 - Check the program and transfer it to the drive
9:25 - Run the program
9:55 - Operational mode

➡️ For more information see:
• ATV320 - ATV Logic manual  NVE71954 (English), NVE71955 (French), NVE71957 (German), NVE71959 (Spanish), NVE71958 (Italian), NVE71960 (Chinese)
Or press "F1" when you are inside the ATV Logic zone in the ATV320 DTM

• ATV320 Programming manual    NVE41295 (English), NVE41296 (French), NVE41297 ​​​​​​​(German), NVE41298 (Spanish), NVE41299 ​​​​​​​(Italian), NVE41300 (Chinese)

 

Schneider Electric USA

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Explore more
Range:
move-arrow-top